Dear friends,
I am developing a project whit the MIMXRT1052. For the initial tests, I am using the SDK for MCUXpresso. I am testing the example evkbimxrt1050_semc. This example is running normaly, but the console isn’t print the text of the debbug. When I create a simple project, as a Hello Word, the console print normaly, but when I use the SDK example, the console no print. Please, I need your help.
PS.: I am using the QSPI Flash (I altered the resistors for the selection). The my QSPI Flash is the IS25LP128.
Best Regards.
Rubens Júnior
解決済! 解決策の投稿を見る。
Hi Rubens Junior
Could you confirm that you have the example code set with the semihosting enabled? you can go to the Quick settings>>SDK Debug Console>>Semihost Console:
Best regards
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------
Hi Rubens Junior
Could you confirm that you have the example code set with the semihosting enabled? you can go to the Quick settings>>SDK Debug Console>>Semihost Console:
Best regards
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
-------------------------------------------------------------------------------
Dear Jorge,
Thankyou very much! It's correct.
Best Regards,
Rubens Júnior