Dear sirs,
While trying to use the SDK example frdmkw41z_wireless_examples_thread_end_device_freertos (but it happen also with router eligible thread end device) I can join the device to the thread network created with Openthread but every time I try to send something pushing a button the KW41Z enter in an hard fault condition.
Querying the board though serial port works.
I'm not able to debug the Hardfault cause it point to strange stack position.
Does anyone have some advice?
Best
Alessio
Hi,
Do you just use the example without any modification ?
Have a great day,
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi, yes, it's a brand new demo project. No edit in the files. The network leader is an OpenThread based border router with a nrf52840 RCP.
With other development board from Nordic the network works without issues.
Best