I need SDK support for the LPC54S616J512BD100.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

I need SDK support for the LPC54S616J512BD100.

734 Views
rudolf_krebs
Contributor I

The 100Pin package is not included in the SDK_2.2_LPC54S616J512.zip-file from 25th of may 2018.

Where can I get the necessary header-files ? Or is there a workaround ?

0 Kudos
Reply
1 Reply

601 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Rudolf,

Thank you for your interest in NXP LPC product, I would like to provide service for you.
Please tell me where you get the LPC54S616J512 100pin package information?
I just find LPC54S616J512BD208 and LPC54S616J512ET180 in our nxp website, and both two chips are NA now, I even don't have the according user manual and datasheet.
I think this is the new chip which is not avaiable now, so the according file is still not avaiable.
If you are sure we have the LPC54S616J512 100 pin package, please tell me where you get the information.


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply