I do intend to use file system Fatfs on a SD card with LPC54608. I don't find SD card driver in "SDK_2.0_LPCXpresso54608\device\LPC54608\drivers" directory. Where Can I find driver for SD Card? Best Regards Giovanni

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I do intend to use file system Fatfs on a SD card with LPC54608. I don't find SD card driver in "SDK_2.0_LPCXpresso54608\device\LPC54608\drivers" directory. Where Can I find driver for SD Card? Best Regards Giovanni

1,428件の閲覧回数
giannigrondona
Contributor III

I am usind SDK_2.0_LPC_EXPRESS 

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 返信

1,222件の閲覧回数
bin_er
NXP Employee
NXP Employee

Hi Gianni Grondona 

In middleware folder, sdmmc_2.1.2, there is fsl_sd.c which is the middleware for SD access.

And in driver folder, fsl_sdif.c is the driver

0 件の賞賛
返信