User segment in flash in Kinetis 64 (frdm kinetis)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

User segment in flash in Kinetis 64 (frdm kinetis)

1,510件の閲覧回数
mikaelelharrar
Contributor III

Hi,

I'm using freedom dev. board FRDM K64 and would like to define a user segment in my flash in order to store there some application data.

Someone knows how to do that ?

Because the main constraint is to avoid the (future) bootloader and the jtag to not erase this segment.

For your information I'm using kinetis studio.

One important other question:

- What is the minimum size of a flash segment ? I see 4K, but is it possible to write only some bytes only or I need to erase all the block each time I want to write on it ?

 

Thanks

Mikael

ラベル(1)
タグ(2)
0 件の賞賛
返信
0 返答(返信)