Hi I am working on LPCXpresso54608. I am running on an example to control LED in the shell. But there is an error when assert(serialHandle); with the error message captured
ASSERT ERROR " .fsl_shell.c:820 : serialHandle
The code that I am using is generated by MCUXpresso.
Thank You!
Hi Alan,
Could you please share the detailed process you are following so I can replicate this issue on my side?
Best regards,
Felipe
Also getting same problem running frdmkl27z_shell example project straight out the box from the frdm_kl27z demo examples.
The example is being run in the default DEBUG configuration.
The other semihosting example called frdmkl27z_hello_world works perfectly.
The Assert fails because SerialHandle is null.
If Alan found a fix I would be interested to know what it is.
Hi Alan,
The solution is to ensure that;
SDK Import Wizard -> SDK Debug Console = UART (not Semihost! The default)
as shown below.
(Also you need to give the second attempt at importing this project a suffix so that the [Next] and [Finish] buttons are ungreyed - allowing you to proceed.)
The imported project settings do NOT control the "SDK Debug Console" setting. You have to set it manually.
Regards, and Thank you Felipe,
Rob
Hi Alan,
I checked the example on my side using my LPCXpresso54608 board and it worked as expected. Please check the below image.
I used MCUXpresso 11.1.1 and SDK 2.7.0 to test it.
Best regards,
Felipe