There is the problem i met when i using GNU Arm Embedded Toolchain to build the SDK package example project in Keil.
Changing settings i did as follows.
1. Using this.
2. Click this and include the path of the GNU Arm Embedded Toolchain I installed.
3. Changing the startup file as the one below the SDK_2.7.0_MIMXRT1052xxxxB\devices\MIMXRT1052\gcc.
4. Setting the Option.(Others stay default)
And now, I build it.
And it will cause some errors like this as follow.
But the startup_MIMXRT1052.S file seems normal.
I am so confuse and hope someone can help me with this problem.
Hi Ethan Guo,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Firstly, I'd like to suggest you check your question, as I didn't see any attachment to this question, secondly, the SDK library has provided the Arm® GCC version of the demos, and please refer to the attachment to test it.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------