1060 I2C with 1 master and 3 slave

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1060 I2C with 1 master and 3 slave

586 Views
sgandhavalla
Contributor I

------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------------

0 Kudos
1 Reply

500 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi  sri naga chaitanya gandhavalla ,

  Please download the RT1060 SDK code, you will find the related I2C slave 

Welcome | MCUXpresso SDK Builder 

  Then you can find the I2C master code from these path:

SDK_2.7.0_EVK-MIMXRT1060\boards\evkmimxrt1060\demo_apps\bubble_peripheral

SDK_2.7.0_EVK-MIMXRT1060\boards\evkmimxrt1060\driver_examples\lpi2c\

bubble_peripheral is very useful to you, as this project will use the I2C master to communicate with the I2C FXOS slave like you.

Wish it helps you!

If you still have questions about it, please kindly let me know.

Kerry

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos