peripherals+ view is empty

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

peripherals+ view is empty

1,680 Views
mastupristi
Senior Contributor I

I have installe KSDK 2.2 for FRDM-K64 but peripherals+ view is empty

Schermata del 2017-05-04 18-08-53.png

In the project preferences I have set correctly the MCU

Istantanea_2017-05-04_18-12-45.png

Where am I wrong?

Best regards

Max

Labels (1)
0 Kudos
Reply
3 Replies

1,426 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Is this actually an IDE created project - did you actually use the "Import SDK examples" or "New project" options in the Quickstart Panel? If you created it via other mechanisms, then it is quite probable that the appropriate settings and linkages are not in place.

Regards,

MCUXpresso IDE Support

0 Kudos
Reply

1,426 Views
mastupristi
Senior Contributor I
Is this actually an IDE created project - did you actually use the "Import SDK examples" or "New project" options in the Quickstart Panel? If you created it via other mechanisms, then it is quite probable that the appropriate settings and linkages are not in place.

It is a project that works fine in KDS 3.2, it a makefile project, and in KDS I can debug and access periphreral registers through EmbSys register view. I tryed to to import it (Existing code as Makefile project) in MCUXpresso ide, the I setup MCU as depicted by screenshots, but something is missing, since the peripherals+ view is still empty.

best regards

0 Kudos
Reply

1,426 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi,

I use P&E OpenSDA interface with FRDM-K64F. There is no problem to check registers in prepheral+ window. See attached video.

I also attach the FRDM-K64F P&E OpenSDA interface I am using.

How it works if you follow the same steps?


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply