impossible to download MCUXPRESSO IDE, I arrive in my login page and stop

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

impossible to download MCUXPRESSO IDE, I arrive in my login page and stop

3,507件の閲覧回数
patricklemoulec
Contributor I

I cannot download MCUXPRESSO IDE

0 件の賞賛
16 返答(返信)

2,808件の閲覧回数
andybeeson
NXP Employee
NXP Employee

I believe that this may be an issue with your account -> especially if your account was created before the NXP/Freescale merger. In this case you may need to create a new account (using a different email address), or else request your account to be reset...

can't download lpcxpresso from download page. 

0 件の賞賛

2,808件の閲覧回数
pavel_sadek
NXP Employee
NXP Employee

Alice

I have checked the link for the Win case, all works ok for me using external network connection.

Pavel

0 件の賞賛

2,808件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi all,

If still have people can't download MCUXpresso, or someone checked this thread that can't

download it , please refer to here :

https://community.nxp.com/docs/DOC-334075 

There will be person help you re-active your account .

BR

Alice

0 件の賞賛

2,808件の閲覧回数
claudiorisi
Contributor I

Hi Alice,

I have exactly the same issue with the download as the other guys on this thread. The product download screenshot with the list of software you have above never comes up and i am taken back to my account screen everytime.

I have checked i am logged in correctly.

I have tried two different browsers, IE11 and Firefox 45.6.0.

Can you post a link to the actual download file rather than the download page please?

Thanks

Claudio

Arrow UK

0 件の賞賛

2,808件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Claudio, 

I have reactivated your account can you please test once more using the link below:

http://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCUXPRESSO 

Out system deactivates users that have not logged in to the page after 14 months. 

Regards,

0 件の賞賛

2,807件の閲覧回数
claudiorisi
Contributor I

This page never comes up. I have copied from your instructions.

pastedImage_7.png

0 件の賞賛

2,808件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi All,

Please use other browsers to have  a try .

I use firefox . There is the same question maybe you can check .

https://community.nxp.com/thread/447608  

0 件の賞賛

2,808件の閲覧回数
patricklemoulec
Contributor I

Other brothers same problem

I finally copy IDE from one collegue

Thanks

0 件の賞賛

2,808件の閲覧回数
claudiorisi
Contributor I

I told you already I have tried Firefox.

0 件の賞賛

2,808件の閲覧回数
EmilioBrivio
Contributor III

The same problem ...login page than my name on the top but asap I change page as you describe step by step the name is not present anymore just only account but in any case following step by step at the end same login page...

Actually I'll use the download made by my colleague same step and all is working ...I'm using windows10..

0 件の賞賛

2,808件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Emilio,

I have gone to your account and I don't see an issue on yours can you please retest with the link below:

http://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCUXPRESSO 

Regards,

0 件の賞賛

2,808件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Patrick,

Please download it at here :

MCUXpresso IDE|NXP 

And please be sure your network is working well .

If still can't download it , please show the error or copy it from others .

BR

Alice

0 件の賞賛

2,808件の閲覧回数
patricklemoulec
Contributor I

Hi Alice,

I have the same problem

I arrive to my login home page and nothing is downloaded

Regards

Patrick

0 件の賞賛

2,808件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi Patrick, 

I have reactivated your account can you please test once more using the link below:

http://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=MCUXPRESSO 

Out system deactivates users that have not logged in to the page after 14 months. 

Regards,

0 件の賞賛

2,808件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi,

After it show the view you shared , please refer to my below screenshots to find the software again.

then it can be download .

pastedImage_1.png

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

pastedImage_5.png

pastedImage_7.png

Please have a try .

BR

Alice

0 件の賞賛

2,808件の閲覧回数
patricklemoulec
Contributor I

Hi Alice,

Unfortunately, after typing download during following step, I comme back again to my login screen!

https://community.nxp.com/servlet/JiveServlet/downloadImage/2-892766-180599/pastedImage_5.png <https://community.nxp.com/servlet/JiveServlet/showImage/2-892766-180599/pastedImage_5.png>

Regards

Patrick

0 件の賞賛