iMXRT SDK 2.11.1 with MCUXpresso 11.4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

iMXRT SDK 2.11.1 with MCUXpresso 11.4

591 Views
Sam_ECU
Contributor V

Hello,

Due to the GCC compiler I'd like to continue to work in MCUXpresso 11.4.  But the SDK's don't install (Null 0,0,0)

Sam_ECU_0-1715966556006.png

 

Sam_ECU_1-1715966576547.png

 

How can I resolve?

0 Kudos
Reply
4 Replies

564 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Sam_ECU,

Please try building and downloading the v2.11.1 SDK package from the SDK builder rather than directly via the IDE. Here is the link for the SDK builder: Select Board | MCUXpresso SDK Builder (nxp.com)

Let me know if you continue experiencing issues.

BR,
Edwin.

0 Kudos
Reply

547 Views
Sam_ECU
Contributor V

Hello @EdwinHz 

They won't install either.  I tried with the newest and oldest available.

I uninstalled MCUXpresso 11.4 (and deleted all directories, program files) and reinstalled, but it has the same issues.

Sam_ECU_2-1716359212812.png

Sam_ECU_0-1716359172015.png

Sam_ECU_1-1716359187798.png

Here the settings:

Sam_ECU_3-1716359550413.png

 

I also tried giving 11.4 it's own directory for the SDKs, but I get the same errors:

Sam_ECU_4-1716359931375.png

 

Regards,

Sam

0 Kudos
Reply

545 Views
Sam_ECU
Contributor V

Hallo Edwin,

I found this information here:

https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools...

Sam_ECU_0-1716362155152.png

Is that the issue? If so, how can I get SDK v2.10 for iMXRT1062?

0 Kudos
Reply

542 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @Sam_ECU,

Yes, MCUXpresso IDE version 11.4 has synchronization for SDK v2.10 or earlier, so the SDK versions that you were trying to install do not work with your IDE, which caused the errors you were seeing. You can use the SDK builder to download SDK v2.10 for the RT1060, you just need to make sure you select the "A" version of the RT1060 to be able to select SDK v2.10:

EdwinHz_0-1716400493461.pngEdwinHz_1-1716400539596.png

BR,
Edwin.

0 Kudos
Reply