Hi fellas,
I'm using MCUXpresso IDE in Ubuntu 20.04. I was able to flash the board and all. In order to detect the serial comm, I was unable to detect the board @ /dev/ttyACM0.
While fro the dmesg logs, the EVK has been enumerated as ttyACM0. This has been a quite a issue and kindly aid to resolve it asap.
已解决! 转到解答。
Hi @GanesanGuru ,
You can search on internet. There is many discuss about /ttyACM0 not appear. It seems this problem is about driver.
Regards,
Jing
Hi @GanesanGuru ,
My system is Ubuntu 20.04 too. But it seems work fine. I use Screen, no problem with it. Please check your system.
When USB connected, it will also enmurate a virtual disk and pop up a bar inform that RT1010-EVK disk is connected. Do you see it?
Regards,
Jing
Hi @jingpan ,
The device is enumerated as follows:
[26164.502922] usb 3-1: SerialNumber: 02320000152ec3b700000000000000000000000097969905
[26164.505986] usb-storage 3-1:1.0: USB Mass Storage device detected
[26164.506065] scsi host0: usb-storage 3-1:1.0
[26164.507962] cdc_acm 3-1:1.1: ttyACM0: USB ACM device
But, when given, sudo screen /deV/ttyACM0, I'm getting Cannot execute '/de/ttyACM0' : No such file or directory and screen terminates.
It would be really helpful, if you've mentioned/shared screenshot of how did you managed to connect to DevKit via Screen in terminal, rather than depicting the devkit enumeration @jingpan
Hi @jingpan ,
The EVK is enumerated as ttyACM0, as shown in dmesg logs
Device is able to code & debug too, as shown in IDE,
When looking for ttyACM0 device @ /dev directory, there is nothing.
Later on debugging the IDE - Its showing as,
Hence, for the same /dev/hidraw0 -- "screen /dev/hidraw0 115200" results in screen is terminating
What am I missing here?!