Hi fellas,
I'm using MCUXpresso IDE in Ubuntu 20.04. I was able to flash the board and all. In order to detect the serial comm, I was unable to detect the board @ /dev/ttyACM0.
While fro the dmesg logs, the EVK has been enumerated as ttyACM0. This has been a quite a issue and kindly aid to resolve it asap.
解決済! 解決策の投稿を見る。
Hi @GanesanGuru ,
You can search on internet. There is many discuss about /ttyACM0 not appear. It seems this problem is about driver.
Regards,
Jing
Hi @GanesanGuru ,
My system is Ubuntu 20.04 too. But it seems work fine. I use Screen, no problem with it. Please check your system.
When USB connected, it will also enmurate a virtual disk and pop up a bar inform that RT1010-EVK disk is connected. Do you see it?
Regards,
Jing
Hi @jingpan ,
The device is enumerated as follows:
[26164.502922] usb 3-1: SerialNumber: 02320000152ec3b700000000000000000000000097969905
[26164.505986] usb-storage 3-1:1.0: USB Mass Storage device detected
[26164.506065] scsi host0: usb-storage 3-1:1.0
[26164.507962] cdc_acm 3-1:1.1: ttyACM0: USB ACM device
But, when given, sudo screen /deV/ttyACM0, I'm getting Cannot execute '/de/ttyACM0' : No such file or directory and screen terminates.
It would be really helpful, if you've mentioned/shared screenshot of how did you managed to connect to DevKit via Screen in terminal, rather than depicting the devkit enumeration @jingpan
Hi @GanesanGuru ,
Sorry but in your first post you said "While fro the dmesg logs, the EVK has been enumerated as ttyACM0". What's it mean? Did you compare with my log?
Regards,
Jing
Hi @jingpan ,
The EVK is enumerated as ttyACM0, as shown in dmesg logs
Device is able to code & debug too, as shown in IDE,
When looking for ttyACM0 device @ /dev directory, there is nothing.
Later on debugging the IDE - Its showing as,
Hence, for the same /dev/hidraw0 -- "screen /dev/hidraw0 115200" results in screen is terminating
What am I missing here?!
Hi @GanesanGuru ,
You can search on internet. There is many discuss about /ttyACM0 not appear. It seems this problem is about driver.
Regards,
Jing