I have a big project which is created on IAR platform, but I have to transfer open source ide like code warrior,MCUXpresso. How to success it? If you lead the way, I appreciate to you.
Microprocessor: MKE04128
best regards,
Hi Alice,
Thank you very much for your helps. Again, I have trouble. I transfered my code blocks from iar to KDS and i gave the necessary paths. And i have some troubles. I have attached the screen shoots.
My problems
"CM0_ics.h"
"CM0_sim.h"
"CM0_ftm.h"
"CM0_pit.h"
"CM0_pwt.h"
CM0_gpio.h"
"CM0_adc.h"
"CM0_i2c.h"
"CM0_spi.h"
"CM0_uart.h"
"CM0_wdog.h"
"CM0_flash.h"
"CM0_kbi.h"
Thank you so much Alice_Yang for your answer. But I have some problems about your recommendation.
1) If I carry my project files form iar to kinetis design studio or mcuxpresso, Do I have to rebuild driver layers and startup files,
2) If rebuild is necessity, how do i make it?
Hi,
-What about your drivers ? If SDK from NXP, there is no need porting the driver layers, there is
SDK version for KDS and MUCpresso IDE.
If others , yes, also import them into new IDE.
- Create a new bare project , copy the drivers and application into it , build ,refer to error message to change,
until there is no error when build. I don't know other direclty way to porting from IAR to KDS.
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello CAN CETIN,
There isn't a directly to convert IAR project to CW or MCUXpresso .
I recommned you create a new project on MCUXpresso , then copy the application
files and code into it .
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------