change flexSPI LUT size

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

change flexSPI LUT size

ソリューションへジャンプ
904件の閲覧回数
adi2Intel
Contributor III

Hi

using SDK example "flexSPI_nor_polling_transfer"

 

I need to set more commands on the LUT.

the costume LUT size is 60 and if the step is 4 between each command, I can only use 15 commands.

I need to use more to support this FLASH device : W25Q128FV pdf, W25Q128FV Description, W25Q128FV Datasheet, W25Q128FV view ::: ALLDATASHEET :::

but if I set the table size to 80, any value after 60 is ignored\not working even after I change the define:

#define CUSTOM_LUT_LENGTH 60

 

any help?

Adi

Intel

0 件の賞賛
返信
1 解決策
854件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @adi2Intel 

The size of LUT is 256, so only support 16 sequences. 

Alice_Yang_0-1680080174726.png

 

BR

Alice

 

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
884件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @adi2Intel 

Which chip are you using? And describe your question more detail, thanks!

 

BR

Alice

0 件の賞賛
返信
881件の閲覧回数
adi2Intel
Contributor III

MX1052

sorry. forgot to mention

0 件の賞賛
返信
855件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello @adi2Intel 

The size of LUT is 256, so only support 16 sequences. 

Alice_Yang_0-1680080174726.png

 

BR

Alice

 

0 件の賞賛
返信