What needs to change when LPCXpresso project is imported into MCUXpresso?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

What needs to change when LPCXpresso project is imported into MCUXpresso?

682 次查看
anaseem
Contributor IV

I imported LPCXpresso project to MCUXpresso IDE.  In MUCXpresso IDE project settings I noticed following setting:

Should I change this setting to MCUXpresso Style?

What other settings need to change ?

Regards,

1 回复

501 次查看
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Amer,

You can find more information about the difference between these two settings in the sections 17.10.1 and 17.10.2 in the MCUXpresso User guide. You might also find this post useful:

https://community.nxp.com/message/980370 

It is also recommended to delete the debug connections and let the MCUXpresso auto discovery functionality to create it again.


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer