By default, MCUXpresso IDE associates .map files with its Map File Editor.
This tool seems to be a bit buggy and cannot handle large .map files (~15MBytes) without long delays or the JVM running out of memory. At least on my machine - Windows 10, 16GBytes of RAM. My colleague's Windows 7 machine with 12 GBytes RAM did not get these excessive delays (but obviously it still took time to read the file). We could not see any obvious/related difference in the MCUXpresso settings. Nearly all settings are the default anyway.
MCUXpresso seems to need to process the .map files whenever it opens a workspace (containing a project with a large .map file), as well as when building and debugging the project. And debugging rarely recovered.
I have to associate all .map files to Text Editor to prevent this problem.
What would be really useful is some documentation to tell me why we need a Map File Editor?
- What errors is it looking for that the compiler/linker do not find?
- What is the purpose of 'editing' a .map file when it is just the human-readable translation of the binary?
- What else does it provide?
I don't want to blindy disable a tool that could potentially be very useful.
I didn't find anything obvious when I searched google or the MCUXpresso help pages.
Thanks!
 
					
				
		
 lpcxpresso_supp
		
			lpcxpresso_supp
		
		
		
		
		
		
		
		
	
			
		
		
			
					
		Duplicate thread. Response posted at https://community.nxp.com/thread/519693#comment-1242461