Usability Issue: File Compare "Cancel" in SDK Component Management

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Usability Issue: File Compare "Cancel" in SDK Component Management

Jump to solution
1,255 Views
danielholala
Senior Contributor II

Hello,

I'd like to suggest a change in handling "Cancel" button during a run of the "Refreshing SDK Components" wizard.

After installing an updated SDK version, it's possible to apply the updates to existing projects that use this SDK, see "MCUXpresso IDE User Guide" , section 7.1 ("SDK Project Component Management example").

When the updates are applied to project files, differences may occur which need to be handled manually. In this case the user is asked to decide to either "Replace", "Keep existing" oder "Compare".

danielholala_1-1643194075439.png

If the user selects "Compare", the file compare utility will open:

danielholala_0-1643194011040.png

The issue: If the user presses "Cancel" to abort comparison, the file is silently not replaced and the update mechanism continues with the next file. That is unexpected and probably not what the user wants. 

Therefore: I suggest to return to the previous state, i.e., this window, to allow the user to explicitly decide what to do with this file:

danielholala_1-1643194075439.png

 

Does that make sense to you?

Best regards,
Daniel

 

0 Kudos
Reply
1 Solution
755 Views
danielholala
Senior Contributor II

This issue has been fixed with MCUXpresso IDE v11.7.0

Thanks!
Daniel

 

View solution in original post

0 Kudos
Reply
2 Replies
1,238 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Hi,

This sounds reasonable. We'll add it to our feature request list for a next release.

Regards,

MCUXpresso IDE Support

756 Views
danielholala
Senior Contributor II

This issue has been fixed with MCUXpresso IDE v11.7.0

Thanks!
Daniel

 

0 Kudos
Reply