Trouble with GPIO_PinInit()

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Trouble with GPIO_PinInit()

942件の閲覧回数
tcwong
Contributor III

I want to use the function GPIO_PinInit to initialize the PTA7 (located in GPIOA). I am using GPIO_PinInit(GPIOA, 7u, &output_config) and I keep getting errors. I already have output_config defined with

gpio_pin_config_t = {

kGPIO_DigitalOutput,

0,

}'

What am I missing? The issue seems to be with GPIOA part of my function.

0 件の賞賛
返信
3 返答(返信)

812件の閲覧回数
FelipeGarcia
NXP Employee
NXP Employee

Hello Tyler,

 

Could you please specify the MCU you are working on? Also, I need to know the errors you are having. Could you please attach a snippet?

 

Best regards,

Felipe

0 件の賞賛
返信

812件の閲覧回数
tcwong
Contributor III

Hello Felipe,

I actually figured out the issue I was having. The first part of the function I should have been using kPGIO_PORTA from the SDK i downloaded. Thanks for trying to help though!

Best,

Tyler

0 件の賞賛
返信

812件の閲覧回数
marek-trmac
NXP Employee
NXP Employee

Hi Tyler,

just a note - there is also supported Pins tool allowing to generate pins configuration for you. The Pins tool cis integrated directly in MCU IDE or available in standalone MCUXpresso Config Tools.

Regards

Marek

Regards,
Marek
0 件の賞賛
返信