Hi Guys,
I want to use the NFC development board OWRCLEV6630B to run NFC demo.
First , I download the latest IDE MCUXpresso 11.3.1.Then I download the latest NFC reader library 06.10.00 (SW297852).After I import the SW297852.ZIP to the IDE and build anyone project , no one could build success.
Finally , I get the previous version 05.22.00 for NFC reader library . It's Okay to import and I solve the build Error. When I debugging the project , code could download in the LPC1769 but IDE couldn't start debug. MCUXpresso report Active faults.
How could I solve this problem? How could I run the latest NFC reader library in MCUXpresso?
Hi NXP support,
Can you guys please confirm that whether clrc663 reader supports listen mode with ios device or not. Recently i was reading ECP support for example for ios and i saw that listen mode is not available for RC663 reader. Kindly confirm whether it's true or not.
Thanks
Sandeep Pawar
Hi @Sandeep_Pawar ,
As far as I know, RC663 can not simulate itself as a card, please kindly refer to the following for details.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi NXP support,
Thanks for your quick reply.
Actually i am able to read data from Andoid device coming towards clrc663 reader that means it is able to detect android smartphone nfc but when i am trying with ios device, i feel like clrc663 is not able to detect ios device nfc i am not sure whether it is possible or not. I have read something about ios device nfc support and i came to know about VASUP-A command now i am looking your guidance for the same.
Sincere Thanks
Sandeep Pawar
Hi @Kan_Li ,
I import library as you show. The problem is also exist
Then I unpacked the ZIP and copy the library folder(ComplianceApp、Example、NxpNfcRdLib、Platform、RTOS) to IDE workspace.(not use import project(s) from file system button )
And I import the exist project one by one. Finally it works
Thanks for your help !
But there is another problem, could you please give me some advise if you have some experience?
When I run the NFC example Nfcrdlib_ISO10373_6_PCD_ComplApp_mcux, I guess this example could read 14443-4A/B card. But the log show error info when I use my Mifare DESFire EV2 4K card close to reader.
Log info :
*** ISO10373-6 PCD compliance example ***
ISO10373-6 PCD application thread started...
Line: 666 Error - (0x0201) has occurred : 0xCCEE CC-Component ID, EE-Error code. Refer-ph_Status.h
Hello @alan_min ,
This demo doesn't support Mifare DESFire EV2 4K cards, you have to use "NfcrdlibEx10_MIFAREDESFire" which is included in the NDA version, you may request it from the doc store with a valid NDA.
Please kindly refer to the attachment for more details.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi @alan_min ,
You may directly send mail to support.docstore@nxp.com for further help with it.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi @alan_min ,
The latest NFC reader library doesn't support archive import, please unzip it at first and refer to the following for details.
Please kindly let me know if the problem is still there.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------