Hello,
the "Terminate and Relaunch" of a debug session result in the following error "There is already a running debug session for the launch configuration". It is not possible to kill this running debug session.
I have to restart MCUXpresso to get it work again. The only way to kill this debug session without restarting is using "Terminate and Remove".
I am using Linux with the lastest MCUXpresso IDE v11.1.1 [Build 3241] [2020-03-02] and a Segger debugger.
I hope someone have a hotfix for this issue.
Thanks a lot and best reagards,
Maximilian
解決済! 解決策の投稿を見る。
Hi,
Could you please try to delete your Launch configuration? With this you put the debug connection settings back to the default.
Regards,
Ricardo
Hi Maximilian,
Hope you are doing well. Did you tried the "Terminate all debug sessions" button?
Also you can use the "Clean up debug" button, it will kill all debug processes associated with the debug connections.
Best Regards,
Ricardo
Hello,
"Clean up Debug" has no effect.
"Terminate all debug sessions" button leads to an error and has no effect on the issue.
I've updated/reinstalled my system to debian 10 but the issue is not solved.
This behavior is really annoying. I hope someone can help me.
Hi,
Could you please try to delete your Launch configuration? With this you put the debug connection settings back to the default.
Regards,
Ricardo
Thanks a lot! This was the solution. :smileyhappy: