Steps to reproduce:
Notice this line has been added:
SYSCTL1 |= SYSCTL1_MCLKPINDIR_MCLKPINDIR_MASK /* Set MCLK Pin as output */
The build fails because the line is missing a semocolon and SYSCTL1 is a pointer. The line should be:
SYSCTL1->MCLKPINDIR |= SYSCTL1_MCLKPINDIR_MCLKPINDIR_MASK;
I'm using MCUXpresso IDE v11.8.0 [Build 1165]. Aside from simply putting this line of code in my own init, are there any suggestions for fixing this?
解決済! 解決策の投稿を見る。
Thanks for reporting this! I was modifying the code myself, but it gets cumbersome when making a repeated changes to clocks, so I just fixed the bug myself.
If anyone else stumbles across this problem, it can be fixed locally by editing line 327 of this file:
mcu_data_v14/processors/MIMXRT685S/ksdk2_0/scripts/clocks/clock_config_c.js
The edit is very straightforward.
Hi @Kenzimatic ,
I think the generated code is wrong, it should be:
SYSCTL1->MCLKPINDIR |= SYSCTL1_MCLKPINDIR_MCLKPINDIR_MASK ;
It is the CFG bug, I will report it it internally, and it will be fixed in the new tool version.
Now, to your side, you can modify the code by yourself.
Thanks a lot for your contribution.
If you find any issues, welcome to let us know.
Best Regards,
kerry
Thanks for reporting this! I was modifying the code myself, but it gets cumbersome when making a repeated changes to clocks, so I just fixed the bug myself.
If anyone else stumbles across this problem, it can be fixed locally by editing line 327 of this file:
mcu_data_v14/processors/MIMXRT685S/ksdk2_0/scripts/clocks/clock_config_c.js
The edit is very straightforward.