Using MCUXpresso IDE v11.2.1 with SDK_2.8.2_MK22FN128xxx12, Redlib (none)
Trying to change stack and heap size from default. When I click on Heap or Stack Size (Default) No dialog is displayed. I've tried --defsym=_HeapSize=0x0100 --defsym=_StackSize=0x0200 in linker flags
My project doesn't use any heap and stack requirements are less the 512 bytes. Currently out of 24K of RAM 7.5K are being consumed by unused heap and stack
>Darren
Have you tried to enter approriate size values in the shown "Settings" screen, instead of leaving it at "Default" ?
There appears no additional screen for me, but I can manually enter values.
Version 11.1. for a LPC546xx, though.