SWO setup by RT1170-EVK MCUXpresso v11.5.0

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SWO setup by RT1170-EVK MCUXpresso v11.5.0

Jump to solution
1,618 Views
auftrag2021
Contributor III

Hello, 

HW: RT1170-EVK

SW: MCUXpressor IDE v11.5.0

SDK: 2.11.0

I upgraded the DAPLink firmware exactly follow the instruction below:

auftrag2021_1-1646098178871.png

Now, a demo program adc_etc_hardware_triffger_conv_cm7 was importet from SDK

The Jumper J22 is connected, SW1 and SW2 are configed as below:

auftrag2021_2-1646098316840.png

But the SWO seemed doesn't work properly

Here is my SWO setup:

auftrag2021_0-1646097953257.png

auftrag2021_3-1646098383231.png

 

Can anyone help, what did I do wrong?

best regards

Siwei

 

 

0 Kudos
1 Solution
1,587 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Hi,

As you noticed on another thread, you can use https://community.nxp.com/t5/Blogs/Overview-of-using-the-MIMXRT1170-EVK-with-MCUXpresso-IDE/ba-p/124... for RT1170-EVK usage with MCUXpresso IDE.

Quoting some information that could help:

lpcxpresso_supp_0-1646315386526.png

lpcxpresso_supp_1-1646315386621.png

DAP-Link mode

lpcxpresso_supp_2-1646315386689.png

LPC-Link2 mode

lpcxpresso_supp_3-1646315386774.png

Regards,

MCUXpresso IDE Support

View solution in original post

0 Kudos
3 Replies
1,570 Views
auftrag2021
Contributor III

Okay, I think I figured out how to enable the SWO, the key is the new firmware LPC-LINK2 must be installed to replace the default firmware, otherwise it won't work. Thank you

0 Kudos
1,588 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Hi,

As you noticed on another thread, you can use https://community.nxp.com/t5/Blogs/Overview-of-using-the-MIMXRT1170-EVK-with-MCUXpresso-IDE/ba-p/124... for RT1170-EVK usage with MCUXpresso IDE.

Quoting some information that could help:

lpcxpresso_supp_0-1646315386526.png

lpcxpresso_supp_1-1646315386621.png

DAP-Link mode

lpcxpresso_supp_2-1646315386689.png

LPC-Link2 mode

lpcxpresso_supp_3-1646315386774.png

Regards,

MCUXpresso IDE Support

0 Kudos
1,581 Views
auftrag2021
Contributor III

I really got confused, if I want enable the SWO debug function in MCUXpresso for my RT1170EVK

1) do need to buy an external hardware debug probe (lpc4322 debug probe) and connect it via JTAG to the RT1170EVK Board?

auftrag2021_1-1646321005210.png

2) or I can barely need to upgrade the firmware on the RT1170EVK debug probe?

If option 2) is possible, how can I upgrade the firmware? 

0 Kudos