Hello,
HW: RT1170-EVK
SW: MCUXpressor IDE v11.5.0
SDK: 2.11.0
I upgraded the DAPLink firmware exactly follow the instruction below:
Now, a demo program adc_etc_hardware_triffger_conv_cm7 was importet from SDK
The Jumper J22 is connected, SW1 and SW2 are configed as below:
But the SWO seemed doesn't work properly
Here is my SWO setup:
Can anyone help, what did I do wrong?
best regards
Siwei
Solved! Go to Solution.
Hi,
As you noticed on another thread, you can use https://community.nxp.com/t5/Blogs/Overview-of-using-the-MIMXRT1170-EVK-with-MCUXpresso-IDE/ba-p/124... for RT1170-EVK usage with MCUXpresso IDE.
Quoting some information that could help:
DAP-Link mode
LPC-Link2 mode
Regards,
MCUXpresso IDE Support
Okay, I think I figured out how to enable the SWO, the key is the new firmware LPC-LINK2 must be installed to replace the default firmware, otherwise it won't work. Thank you
Hi,
As you noticed on another thread, you can use https://community.nxp.com/t5/Blogs/Overview-of-using-the-MIMXRT1170-EVK-with-MCUXpresso-IDE/ba-p/124... for RT1170-EVK usage with MCUXpresso IDE.
Quoting some information that could help:
DAP-Link mode
LPC-Link2 mode
Regards,
MCUXpresso IDE Support
I really got confused, if I want enable the SWO debug function in MCUXpresso for my RT1170EVK
1) do need to buy an external hardware debug probe (lpc4322 debug probe) and connect it via JTAG to the RT1170EVK Board?
2) or I can barely need to upgrade the firmware on the RT1170EVK debug probe?
If option 2) is possible, how can I upgrade the firmware?