SDK for the MIMX8 EVK

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

SDK for the MIMX8 EVK

272 次查看
dmitriyantonets
Contributor I

Hi all,

I had a problem when adding a new SDK.
I use:

MCUXpresso IDE v11.6.1 [build 8255] [2022-10-03],

SDK_2_12_1_MIMX8MM2xxxLZ.zip generated a day ago.

When I try to add this SDK, I get the following message:

Error messageError message

 

The manifest (MIMX8MM2xxxLZ_manifest_v3_10.xml) has the following compiler version requirement:

<toolchain id="armgcc" name="GCC_ARM_Embedded_10-2021.10" version="10.3.1" full_name="GCC ARM Embedded 10-2021.10" compiler="compiler_gcc" type="armgcc" vendor="GCC ARM Embedded" vendor_url="http://launchpad.net/gcc-arm-embedded"/>

Which I do not have installed.
I could not find this old version for the GCC.
I have several later versions cross-compilers for ARM installed which I actively use (e.g. to build Linux for this board with Yocto).
Question - how can I configure to use a different with requirement version of GCC for add this SDK?

Thank you.

0 项奖励
1 回复

258 次查看
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi dmitriyantonets 

Thank you for contacting us.
SDK_2_12_1_MIMX8MM2xxxLZ only supports these two compiler/debugger. MCUXpresso IDE is not supported.

ZhangJennie_0-1671442160167.png

For more see attatched
Getting Started with MCUXpresso SDK for EVK-MIMX8MM.pdf

Chapter 3, Toolchain introduction.

 

Have a nice dya,

Jun Zhang

0 项奖励