Refresh MCU Cache

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Refresh MCU Cache

1,830 Views
jeffthompson
Contributor V

Can someone explain the 'Refresh MCU Cache' button in the MCU Settings page of the project properties? What does it do, and how do I know when to use it? For reference, I'm using MCUXpresso 11.1.0.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

1,750 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello Jeff,

Hope you are doing well.

If a project is built using part support from an SDK and is then exported – for example to share the project with a colleague who also uses MCUXpresso IDE, then the colleague must also install an SDK providing part support for the project’s MCU. Since device support is included in the SDK, it is recommended that any required SDKs are installed before a project requiring SDK part support is imported. However, if this is not done beforehand, simply select the imported project in the project explorer and right click and select: C/C++ Build -> MCU settings ensure the correct MCU is selected and click Refresh MCU Cache.

Hope it helps!

Sabina

-----------------------------------------------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer button. Thank you!

----------------------------------------------------------------------------------------------------------------------- 

0 Kudos
Reply