QN902X support in MCUxpresso

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

QN902X support in MCUxpresso

958 次查看
michelkuenemann
Contributor III

Hi NXP,

I plan to use a QN9020 in a new design and I have two questions:

1 - is this device recommended for new designs ? - if NOT, which device does NXP recommend ?

2 - where can I find the MCUxpresso SDK for this device ?

Thanks a lot

Michel Kuenemann

0 项奖励
回复
3 回复数

809 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Well there is the newer QN device - QN09080

And also in the Kinetis W range, some devices have Bluetooth and MCUXpresso SDKs available 

For more info on supported devices check the mcuxpresso.nxp.com website for downloadable SDKs, plus the MCUXpresso Supported Devices Table 

Regards,

MCUXpresso IDE Support

0 项奖励
回复

809 次查看
lpcxpresso_supp
NXP Employee
NXP Employee

Sorry, there are no plans to support QN9020 in the MCUXpresso environment.

From a quick glance at the product page (QN902x|NXP ) it appears that you will need a copy of IAR or Kei tools, and the QN team provide a product specific SDK (i.e. not an MCUXpresso SDK).

Regards,

MCUXpresso IDE Support

0 项奖励
回复

809 次查看
michelkuenemann
Contributor III

Thanks for prompt reply.

Does NXP provide another BLE SOC which IS supported by MCUXpresso ?

Michel

0 项奖励
回复