Hi, I've been using MCUXpresso for the first time this week, migrating an already started project from KDS and after some research I found about the wonders of MTB and I want to use it, it can save lots of time.
I've read MCUXpresso IDE Instruction Trace and there it all seems as easy as a few clicks, fortunately the mtb.c file is there already and it seems MTB is enabled, even on the map file I can see the symbol _mtb_buffer_ that uses 128 bytes.
So I run my target and suspend it, then I go to the new Instruction Trace view and click on Record Continuously:
I get this message:
So then I open the Instruction Trace Config View and click on Load Config From Target
And I get this message:
Is there anything I'm doing wrong of am I missing something?
Thanks for your help!
This sounds like a reported bug which has been fixed in the next maintenance release. Try this as a workaround.
Once your code reaches the initial breakpoint (typically on 'main'), open the RedlinkServer console, and type 'corelist this'. You'll see a display of core ID, and core type. Next, set the MTB to record continuously. Start execution of your target to allow the trace buffer to fill. Download the trace buffer to make sure the instruction trace is operational. Report your results.
Thanks and regards,
LPCXpresso Support
I'm afraid that the MTB trace support built into MCUXpresso IDE is LinkServer (CMSIS-DAP) only. Please see the supplied MCUXpresso IDE v10.0.0 Instruction Trace Guide for more details.
We do have a long term aim of supporting other probes for MTB trace, but in the shorter term we'll look at capturing the use of other debug probes more cleanly in a future release.
Regards,
MCUXpresso IDE Support