MCUXpressoIDE_11.1.1_3241 is not start in windows 8.1 32bit

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpressoIDE_11.1.1_3241 is not start in windows 8.1 32bit

Jump to solution
1,048 Views
nales1
Contributor I

MCUXpressoIDE_11.1.1_3241 is not start in windows 8.1 32bit 

0 Kudos
Reply
1 Solution
975 Views
ErichStyger
Specialist I

From V11.0.0 on it only supports 64bit, because Eclipse is 64bit only.

Extract from the release notes:

=========================
Version 11.0.0 (Jun 2019)
=========================

* Upgraded underlying Eclipse Framework to 4.10.0v201812 / CDT 9.6.0.

* Upgraded supplied GNU ARM Embedded Toolchain to GCC8 (2018q4-major)

* Windows version of product now only runs on Win64 (IDE v10.3.1 and
  earlier ran on Win32 & Win64 platforms). Note that this change has
  been driven by the fact that Eclipse framework is now 64-bit only.
  [ Ubuntu and MacOS versions of product already only ran on 64-bit
    platforms.]

View solution in original post

1 Reply
976 Views
ErichStyger
Specialist I

From V11.0.0 on it only supports 64bit, because Eclipse is 64bit only.

Extract from the release notes:

=========================
Version 11.0.0 (Jun 2019)
=========================

* Upgraded underlying Eclipse Framework to 4.10.0v201812 / CDT 9.6.0.

* Upgraded supplied GNU ARM Embedded Toolchain to GCC8 (2018q4-major)

* Windows version of product now only runs on Win64 (IDE v10.3.1 and
  earlier ran on Win32 & Win64 platforms). Note that this change has
  been driven by the fact that Eclipse framework is now 64-bit only.
  [ Ubuntu and MacOS versions of product already only ran on 64-bit
    platforms.]