MCUXpresso v11 toolbar height is extremely tiny

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso v11 toolbar height is extremely tiny

Jump to solution
1,258 Views
HPT_Dave
Contributor II

When using a very high resolution display (4K) the MCUXpresso v11 toolbar height is extremely tiny. Is there a way to make it larger.

0 Kudos
Reply
1 Solution
1,209 Views
ErichStyger
Specialist I

I don't have such a display, so cannot try it out. But some of my students had the same problem, so I wrote an article which helped them to solve it:

https://mcuoneclipse.com/2017/10/11/dealing-with-eclipse-and-very-small-icons-on-ultra-high-density-...

Can you check if this works for you?

Erich

View solution in original post

3 Replies
1,210 Views
ErichStyger
Specialist I

I don't have such a display, so cannot try it out. But some of my students had the same problem, so I wrote an article which helped them to solve it:

https://mcuoneclipse.com/2017/10/11/dealing-with-eclipse-and-very-small-icons-on-ultra-high-density-...

Can you check if this works for you?

Erich

1,193 Views
HPT_Dave
Contributor II

That did the trick! Thanks to you and your students for the help!

Dave

0 Kudos
Reply
1,221 Views
Miguel04
NXP TechSupport
NXP TechSupport

Hi @HPT_Dave 

No there isn't a way to zoom in the toolbar, only the text editor.

Here you can zoom in the text editor, in case this also is an issue.

Miguel04_0-1674507118568.jpeg

Let me know if you have another question.

Best Regards, Miguel.