MCUXpresso 11.4.1 Debugger Console. Path for the index cache directory

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCUXpresso 11.4.1 Debugger Console. Path for the index cache directory

ソリューションへジャンプ
1,546件の閲覧回数
luis-martinez
Contributor III

Hi friends,

Someone has this message (apparent error in Debugging Console) when launch Debug action?,...

"C:
xp\MCUXpressoIDE_11.4.1_6260\ide\plugins\com.nxp.mcuxpresso.tools.win32_11.4.0.202103011116 oolsinrm-none-eabi-gdb.exe: warning: Couldn't determine a path for the index cache directory."
(The message is a copy/paste from the console).

It seem a lost in path composition of the path,... but not clear where is the fault and how fix. The debugger seem works (in general),..

Thanks for your comments.

0 件の賞賛
1 解決策
1,524件の閲覧回数
luis-martinez
Contributor III

Hi Alice, many thanks for your link (I don't know why it not appear for me,... it was searched but,...),

About your answer,... apparently debug sessions works well,... it was tested in LPC845max board:

I loaded two full SDK' examples (SDK has been fully update), in both cases the error or warning appear when debug session is started.
1st Example. Demo "led_blinky". It seem work with the warning in the debug console. The debug session start (it activate the error in red text) but tha app run and red led blinks as expected.

2nd Example. Driver "gpio_led_output". It seem works, also, whith the warning in the debug console. As previous the error message is activate when debug start. Green led blinks when SW2 switch is pressed (uart data not tested,...)

Without more information I will closed this issue, if it appear some more data I will inform you.

Thanks.

元の投稿で解決策を見る

タグ(1)
0 件の賞賛
2 返答(返信)
1,529件の閲覧回数
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello luis-martinez,

How about erase all your flash, and download a simple demo project ?

Does the program loaded can work well? If yes, you can ignore it , have a look at the below thread:

https://community.nxp.com/t5/MCUXpresso-IDE/warning-Couldn-t-determine-a-path-for-the-index-cache-di... 

 

BR

Alice

0 件の賞賛
1,525件の閲覧回数
luis-martinez
Contributor III

Hi Alice, many thanks for your link (I don't know why it not appear for me,... it was searched but,...),

About your answer,... apparently debug sessions works well,... it was tested in LPC845max board:

I loaded two full SDK' examples (SDK has been fully update), in both cases the error or warning appear when debug session is started.
1st Example. Demo "led_blinky". It seem work with the warning in the debug console. The debug session start (it activate the error in red text) but tha app run and red led blinks as expected.

2nd Example. Driver "gpio_led_output". It seem works, also, whith the warning in the debug console. As previous the error message is activate when debug start. Green led blinks when SW2 switch is pressed (uart data not tested,...)

Without more information I will closed this issue, if it appear some more data I will inform you.

Thanks.

タグ(1)
0 件の賞賛