I am just starting a project that, for now, will be based on the IMXRT1020-EVK. I downloaded MCUXpresso 11.1.0, and also configured and downloaded the SDK from here. Then I installed the IDE and started it up, and in the Welcome message it gives me the option to download and install SDKs. So I went there figuring it would ask me to point to the SDK that I just downloaded, but it didn't. It gave me a list of SDKs, none of which point to the IMXRT1020-EVK. I assme there must be some what to connect the IDE to the SDK I already downloaded, or there must be a way to have the IDE pick up the IMXRT1020-EVK SDK.
Anyone run into this problem?
Thanks in advance...
解決済! 解決策の投稿を見る。
Hi Ed,
type "1020" into the filter on the right side:I'm using "evkmimxrt1020"
Regards
Marek
Hi Ed,
type "1020" into the filter on the right side:I'm using "evkmimxrt1020"
Regards
Marek
Probably a bit old fashioned, but did your try reading the manual? Hint section 4.2 is a good place to start.
Self-answered...
Ok, looks like I just drag-n-drop the SDK.zip file (SDK_2.7.0_EVK-MIMXRT1020.zip) into the "Installed SDKs" window of the IDE. Then I can reference it when I create the project.