LPC55s69JBD100 Evaluation board : unable to load the program via debug port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LPC55s69JBD100 Evaluation board : unable to load the program via debug port

2,756 Views
Deeps_bang
Contributor III

Hi Team, 

Trying to load 'LPC55s69_Project_I2C' program on the board via p6 debug link.

But, getting  error as 'could not connect to the core. No connection to chip's debug port'.

 

jumper J3 at--> Loc  side.

DFU Jumper attached.

These are the configurations made.

Am I missing anything???

 

Regards,

Deep_Bang

0 Kudos
Reply
11 Replies

2,733 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @Deeps_bang,

Could you please remove the DFU Jumper before connecting the board? Has the problem gone?

Also, is this happening with examples too? Have you modified something else of your board (e.g. the jumper settings)?

Best regards, Raul.

0 Kudos
Reply

2,723 Views
Deeps_bang
Contributor III

Hi Raul,

Thank you for the response.

Ya, DFU jumper removed and connected . problem still exist.

I am trying with example code only now, like hello_world, blinky. Problem still exist.

On jumper setting ,nothing modified. As per requirement P4 is at 3.3v and J3 is at LOC side.

Actually, 6 months back I used this EVK and tested with Blinky program and all, it was working. then i used this board as external debugger.

And used this board in ISP mode also. All that time it was working fine only.

Now, need to use it for some application, so thought to test initial setup with basic program, there itself I am stuck.

 

Now, even i tried with ISP through flashing possibility , using blhost.exe and USB via. But to the hard luck USB ports are not getting enumerated in device manager. The required jumper setting for them maintained via J7 and J6 to try with Full speed or High speed USB. Then i thought to flash through UART at least with P1 jumper intact. Its showing no response to ping command . So, ISP through flashing also not happening.

Do i have to Erase the chip once. If yes, how to do it.??

or anyother solution for this??

 

Thanks & Regards,

Deep_Bang

 

 

 

 

0 Kudos
Reply

2,694 Views
RaRo
NXP TechSupport
NXP TechSupport
0 Kudos
Reply

2,685 Views
Deeps_bang
Contributor III

Hi Raul,

As you suggested, for first option to try , I dont have Segger J-Link.

So, I tried with 2nd  mass erase with GUI Flash tool.  But, still its giving error as could not connect to the core.

No connection to chips debug port. i.e 

Failed on connect: Ee(42). Could not connect to core.
No connection to chip's debug port
(100) Target Connection Failed
Unable to perform operation!
Command failed with exit code 1

 

Regards,

Deep_Bang

0 Kudos
Reply

2,683 Views
Deeps_bang
Contributor III

LPC 55s69 EVK with initial jumper settingLPC 55s69 EVK with initial jumper setting

 

PFA EVK board. As soon as i connect the board via Debug link , the LED near DS1 is on constant and LED near DS2 is blinking. This s the status of board.

If you need anyother information , let me know.

TR

Deep_Bang

0 Kudos
Reply

2,647 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @Deeps_bang,

Could you please try erasing the flash clicking on Erase flash action using… in MCUXpresso IDE?

RaulRomero_0-1696453914124.png

[MCUXpresso IDE v11.8.0]

If that does not work, here are some steps you could try to regain control of your LPC without using an external debugger. For that, you might need to install LPCScrypt v2.1.2 | NXP Semiconductors and J-Link Commander.

Second of all, we need to put the board on DFU. Please put a jumper on J4 to force DFU Mode. Then connect it to the PC.

Afterwards, locate the scripts of LPCScrypt: program_JLINK.cmd. While you have your board plugged in, run the script program_JLINK to flash the firmware. Then remove the USB cable to power down the board and remove the DFU jumper.

Now, connect the board in ISP mode placing a jumper in J10, open J-Link Commander and start the communication by sending the command "connect". After that, use the command "?" to search and select your board on a new popup window (LPC55S69).

Finally, select the interface of communication of the EVK for that write "S" for SWD. On speed just click Enter without an entry. Then use the command "erase". Disconnect the USB to power down the board and remove the ISP jumper, then open MCUXpresso IDE and test the board with a led blinky example.

Best regards, Raul.

0 Kudos
Reply

2,641 Views
Deeps_bang
Contributor III

Hi Raul,

Thank you for the response.

I was doing the steps as you suggested. But, got struck at progarm_JINK.cmd .

PFA .JPG for your reference.

 

Regards,

Deep_Bang

0 Kudos
Reply

2,639 Views
Deeps_bang
Contributor III

HI,

FYI , I tried tried with all the USB ports, starting from Debug link(P6), then High  speed, Full speed,

 even just power supply port. For all same Message as in .JPG  

0 Kudos
Reply

2,571 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @Deeps_bang,

Actually, 6 months back I used this EVK and tested with Blinky program and all, it was working. then i used this board as external debugger.

And used this board in ISP mode also. All that time it was working fine only.

Could you please tell us if you modify something of the board to work as external debugger and ISP mode? We have noticed that you have J5 on the board. Have you used it before?

Also, just for double check, could you please try with other USB cable to P6 and verify that the jumper in J4 (DFU) is installed properly?

Finally, do you have an external debugger that we could use to connect the LPC4322 through P7? For example, an MCU Link JTAG/SWD Debug Probe | NXP Semiconductors?

Best regards, Raul.

0 Kudos
Reply

2,555 Views
Deeps_bang
Contributor III

Hi Raul,

I could do the LPCScrypt program_JLINK .cmd execution . The DS2 LED is not blinking now. 

Where as when I tried with next steps with respect to J10 jumper insertion + reset to be in ISP mode and J_link commander , now I got struck here as attached .JPG for your reference. In this commander window 

when it comes to device selection it gives two options LPC55s69

Deeps_bang_0-1696572682941.png

which one to select exactly. Actually i tried with both but getting same response as shown in .jpg

 

*Then, now in MCUXpesso IDE CMSIS-DAP probe not getting detected . JLink_SEGGER probe was detectable. I tried to debug with that probe, Erase with that probe . But could not do it , attached .jpg for your reference.

"Could you please tell us if you modify something of the board to work as external debugger and ISP mode? We have noticed that you have J5 on the board. Have you used it before?"

No, modification done to the board. We used the board for external debugging by just shifting jumper   J3 to EXT side. 

* I doubt on whether the device is entering to ISP mode. And, then these High speed and Full speed USB ports are not getting enumerated in Device manager of windows PC.

 

Thanks & Regards,

Deep_Bang

 

0 Kudos
Reply

2,473 Views
RaRo
NXP TechSupport
NXP TechSupport

Hello @Deeps_bang,

Could you please use the J-Link Commander V7.88m?

which one to select exactly

It should work selecting the LPC55S69_M33_0.

Finally, could you please try to do some extra steps as mentioned here: Internal and External Debug Options for the NXP LPC55S69-EVK Board | MCU on Eclipse, there are described extra steps before the usage of J-Link Commander that could help. And, just for double check, do you have any external debugger that we could use to connect the LPC4322 through P7? For example, an MCU Link JTAG/SWD Debug Probe | NXP Semiconductors?

Best regards, Raul.

0 Kudos
Reply