Is there a guide to migrate a project form uVision 5 to MCUXpresso?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Is there a guide to migrate a project form uVision 5 to MCUXpresso?

831 次查看
m4l490n
Contributor V

Hello

Since there is no uVision for Linux, and also uVision is a horrible IDE, I would like to know if there is an official, or unofficial, guide to migrating projects from uVision 5 to MCUXpresso.

Thanks!

标记 (2)
0 项奖励
回复
1 回复

706 次查看
jorge_a_vazquez
NXP Employee
NXP Employee

Hi Manuel Malagon

If you developed the project with our SDK software, then we normally recommend to create a new project in MCUXpressoIDE (with the drivers needed from SDK) and then copy and paste the application (source files) from the Keil project to the MCUXpresso Project. If there is a dependency in the uVision project, then you can add it to the new project in MCUXpresso.

Hope this helps
Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复