Incorrect values are shown in the peripherals+ view when I debug “flexcan interrupt transfer ”of SDK2.2.0 and view the value of CAN0-CTRL1 register with TWRKV46F150M and MCUXPresso v10.0.2 [Build 411]. As shown below, the bit fields named BOFFREC, RWRNMSK, LPB, CLKSRC and ERRMSK only have one bit, but why is the value bigger than 1 shown in the bit fields? What are meaning of “Value_0” or “Value_1”shown in some bit fields?
Hello Eric,
This will be fixed in the next version MCUX_IDE_v10.1.0_PRC2 .
Hope it Helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello Erich,
1. “Value_0” or “Value_1” meaning 0 and 1, you can point to the value, you will see the meaning :
2. About ""the bit fields named BOFFREC, RWRNMSK, LPB, CLKSRC and ERRMSK only have one bit, but why is the value bigger than 1 shown in the bit fields? "
I think there maybe some problem, I will report it to Expert team, and maybe the new version will fix it.
Hope it helps
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------