How to install MCUxpresso IDE 11 on Debian 10 Buster

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to install MCUxpresso IDE 11 on Debian 10 Buster

2,010 次查看
acontini
Contributor I

Hello everyone,

I would like to share with you all my short guide on how to install MCUxpresso 11 on Debian 10.

The NPX website clearly states that Debian >=9 are not supported. There is although a workaround to satisfy all dependancies.

I am currently using Debian 10, but the installation on Debian 9 is more straight forward.

Please test it, provide feedback or even transform it to an automatic script and publish it online. The following text is released under public domain.

Disclaimer: I am providing these commands WITHOUT ANY WARRANTY. I am not able to provide any troubleshooting if things goes wrong. All downloaded packages are from an official source. Use it at your own risk.

1) Multiarch

Activate Multiarch, and in particular the i386 architecture. More info here - https://wiki.debian.org/Multiarch/HOWTO

2) Install dependencies

Before running the MCUxpresso installer, please install the following dependencies:

libncurses-dev

$ sudo apt-get install libncurses-dev:i386‍

libusb-1.0

$ sudo apt-get install libusb-1.0:i386‍

dfu-util

$ sudo apt-get install dfu-util:i386‍

libwebkitgtk-1.0 is the more complex package and it has a lot of dependencies. The following command install the packages already available from the Debian repo.

$ sudo apt-get install libjavascriptcoregtk-1.0-0:i386 libatk1.0-0:i386 libcairo2:i386 libenchant1c2a:i386 libfontconfig1:i386 libfreetype6:i386 libgdk-pixbuf2.0-0:i386 libgl1-mesa-glx:i386 libgl1:i386 libgstreamer-plugins-base1.0-0:i386 libgstreamer1.0-0:i386 libgtk2.0-0:i386 libharfbuzz-icu0:i386 libharfbuzz0b:i386 libicu57:i386 libjpeg62-turbo:i386 libpango-1.0-0:i386 libpangocairo-1.0-0:i386 libpangoft2-1.0-0:i386 libsecret-1-0:i386 libsoup2.4-1:i386 libsqlite3-0:i386 libwebp6:i386 libx11-6:i386 libxcomposite1:i386 libxdamage1:i386 libxfixes3:i386 libxml2:i386 libxrender1:i386 libxslt1.1:i386 libxt6:i386 gstreamer1.0-plugins-base:i386 gstreamer1.0-plugins-good:i386 geoclue-2.0:i386‍

Some packages are not included in the current Debian 10 repository, so we need to fetch them manually.

Create libwebkitgtk.txt

$ echo 'http://ftp.uk.debian.org/debian/pool/main/w/webkitgtk/libwebkitgtk-1.0-0_2.4.9-1~deb8u1_i386.deb
http://security.debian.org/debian-security/pool/updates/main/i/icu/libicu52_52.1-8+deb8u8_i386.deb
http://ftp.uk.debian.org/debian/pool/main/w/webkitgtk/libwebkitgtk-1.0-common_2.4.9-1~deb8u1_all.deb
http://ftp.uk.debian.org/debian/pool/main/w/webkitgtk/libjavascriptcoregtk-1.0-0_2.4.9-1~deb8u1_i386...
http://ftp.uk.debian.org/debian/pool/main/libw/libwebp/libwebp5_0.4.1-1.2+b2_i386.deb
https://downloads.sourceforge.net/project/libpng/libpng12/1.2.59/libpng-1.2.59.tar.gz' > libwebkitgtk.txt‍‍‍‍‍‍

Download the packages for manual installation

$ wget -i libwebkitgtk.txt‍

Cross compile libpng for i386 architecture

$ tar -zxvf libpng-1.2.59.tar.gz
$ cd libpng-1.2.59
$ ./configure --host=i386 --libdir=/usr/lib/i386-linux-gnu/
$ make check
$ sudo make install‍‍‍‍‍

Install libicu52

$ sudo dpkg -i libicu52_52.1-8+deb8u8_i386.deb‍

Install libwebkitgtk-1.0-common_2.4.9

$ sudo dpkg -i libwebkitgtk-1.0-common_2.4.9-1_deb8u1_all.deb‍

Install libwebp5

$ sudo dpkg -i libwebp5_0.4.1-1.2+b2_i386.deb‍

Install libwebkitgtk forcing it to ignore libpng12 dependencies as the correct library is already installed.

$ sudo dpkg -i --force-depends libwebkitgtk-1.0-0_2.4.9-1_deb8u1_i386.deb‍

Install libjavascriptcoregtk

$ sudo dpkg -i libjavascriptcoregtk-1.0-0_2.4.9-1_deb8u1_i386.deb‍

3) Download MCUxpresso IDE and Config Tools

Link: https://www.nxp.com/design/software/development-software/mcuxpresso-software-and-tools/mcuxpresso-in...

Run the bin file as root

$ sudo ./mcuxpressoide-11.0.1_2563.x86_64.deb.bin‍

Clean some space post installation

$ sudo apt autoremove‍

I hope everything has gone as planned.

4) Download the SDK

Download the correct SDK for your device/development board.

5) Import your project or start developing

Have fun! Smiley Happy

标签 (1)
0 项奖励
回复
1 回复

1,925 次查看
Sebastian_Del_Rio
NXP Employee
NXP Employee

Hi Andrea, I hope you're doing well!

Thank you very much for providing this guide and for also providing your feedback, we appreciate it.

Best regards,

Sebastian