Hello,
For the last 2 weeks, I've struggled to add a second QSPI chip to a RT1060EVK dev board. I have posted numerous forum questions and I don't know what the issue is. The app note AN12564, while useful, doesn't actually show you how to modify the code to make the second chip work and the reference manual has a lot of detail, but doesn't explain what needs to happen in code.
On the dev board, we have hooked up a second QSPI device to FlexSPI A. The device is identical to the one already on the board and we set FLEXSPI_A_SS1_B to [H13] GPIO_AD_B1_08.
In software, we are trying to modify the "evkmimxrt1060_flexspi_nor_polling_transfer" project. In the project settings, we added the second flash as "Flash_00" and assigned it to 0x60800000 and a size of 0x800000. We have updated the pin_mux files and added the ".sflashA2Size" command to "xip\evkmimxrt1060_flexspi_nor_config.c". In app.h, the FLASH_SIZE was increased from 0x2000 to 0x4000 and in the project, we modified the flex_spi_flash_init() command to include "FLEXSPI_SetFlashConfig(base, &deviceconfig, kFLEXSPI_PortA2)"
Looking at the memory viewer, I can see that the memory location 0x60800000 seems to contain memory configuration data, but starting at location 0x60802000 I can see the actual A1 program data. Additionally, the A2 chip select signal is not toggling when I try reading the A2 memory locations which tells me that I have a setup issue.
Numerous Questions:
Solved! Go to Solution.
Hello Jing,
Thank you for your project. It still didn't work for me, but I was able to use it to locate my problem. (A combination of the wrong device address and the pin setup.) In case anyone else has the same issue, I'm attaching the version of my example project that I was able to get working.
For people trying to replicate this, the SS1 chip select is routed to J22.4.
Hi @chadgraham ,
But in your code, when calling flexspi_nor_flash_erase_sector() and flexspi_nor_flash_page_program(), it still erase/write kFLEXSPI_PortA1, not kFLEXSPI_PortA2. So, I'm not clearly get what you want. I modified your code, change all A1 to A2 in flexspi_nor_fklash_ops.c, and change EXAMPLE_FLEXSPI_AMBA_BASE definition to 0x60800000. It works well. I can see the right data in 0x60814000.
Can AN12564sw run on your board?
Regards,
Jing
Hello Jing,
Thank you for your input.
Hello Jing,
Thank you for your project. It still didn't work for me, but I was able to use it to locate my problem. (A combination of the wrong device address and the pin setup.) In case anyone else has the same issue, I'm attaching the version of my example project that I was able to get working.
For people trying to replicate this, the SS1 chip select is routed to J22.4.