Hello Alice,
I don't have j-link debug probe. How can I proceed ?
Regards,
Hello @Flo2
Sorry maybe you misunderstood me. I mean update the firmware of OpenSDA to J-link. No external J-link debugger needed.
Pay attention, if your system is win10. Please find a Win7 system PC to update.
Detail please refer to:
BR
Alice
What is the binary file I have to download ? OpenSDA V1 Bootloader ?
Where is the Segger JLink drivers in the download page?
Regards
Hello @Flo2
Steps as below:
1) Find a win7 PC.
2) Pressing RST button of your board, plug-in USB with SDA.
3) There should be a "bootloader" Drive on your PC.
4) Copy and paste the Application binary file into the BOOTLOADER drive. I attach the binary file to you.
5)Un-plug and re-plug the USB cable from the SDA USB port WITHOUT keeping reset button pressed.
BR
Alice
Hello,
Will it works with a Windows 11 ?
Regards
Hello @Flo2
Update firmware need based on Win7 system.
After updated, board can work on Win11.
If you really no Win7, can try this method:
https://mcuoneclipse.com/2018/04/10/recovering-opensda-boards-with-windows-10/
BR
Alice