Hi,
I am using MCUXpresso IDE v10.1.0 [Build 589] with SDK 2.3.0 . When I tried to load the SDK examples emwin examples are missing. I have downloaded the SDK including the EMWIN components.
Whether the MCUXpresso IDE v10.1.0 [Build 589] doesn't support emWin?
Thanks & Regards,
Anjali
You need to use the latest SDK 2.4.0 release to get access to emwin. This will also mean updating the MCUXpresso IDE v10.2.
To download the SDK 2.4.0 for i.MX RT1050, visit https://mcuxpresso.nxp.com
For details of MCUXpresso IDE v10.2, see: MCUXpresso IDE v10.2.0 Now Available
Regards,
MCUXpresso IDE Support
Is there any way I can use the mcuexpresso for sd card flashing. I tried converting afx file to bin and use elftosb utility to generate sb file and flash the same to SD card. But in mcuexpresso the linker file is created only for hyperflash ,if I edit its contents whether SD card booting is possible.?
The SDK for which MCU?
Note that the current releases are MCUXpresso IDE v10.2 and SDK 2.4.0.
Regards,
MCUXpresso IDE Support