EMWIN SUPPORT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

EMWIN SUPPORT

1,295 Views
anjalikkrishna
Contributor III

Hi,

       I am using MCUXpresso IDE v10.1.0 [Build 589] with SDK 2.3.0 . When I tried to load the SDK examples emwin examples are missing. I have downloaded the SDK including the EMWIN components. 

  

Whether the MCUXpresso IDE v10.1.0 [Build 589]  doesn't support emWin?

Thanks & Regards,

Anjali

0 Kudos
4 Replies

940 Views
lpcxpresso_supp
NXP Employee
NXP Employee

You need to use the latest SDK 2.4.0 release to get access to emwin. This will also mean updating the MCUXpresso IDE v10.2.

To download the SDK 2.4.0 for i.MX RT1050, visit https://mcuxpresso.nxp.com

For details of MCUXpresso IDE v10.2, see: MCUXpresso IDE v10.2.0 Now Available 

Regards,

MCUXpresso IDE Support

0 Kudos

940 Views
anjalikkrishna
Contributor III

Is there any way I can use the mcuexpresso for sd card flashing. I tried converting afx file to bin and use elftosb utility to generate sb file and flash the same to SD card. But in mcuexpresso the linker file is created only for hyperflash ,if I edit its contents whether SD card booting is possible.?

0 Kudos

940 Views
lpcxpresso_supp
NXP Employee
NXP Employee

The SDK for which MCU?

Note that the current releases are MCUXpresso IDE v10.2 and SDK 2.4.0.

Regards,

MCUXpresso IDE Support

0 Kudos

940 Views
anjalikkrishna
Contributor III

The MCU is MIMXRT1050-EVK .Silicon Revision is  A0

Thanks & Regards,

Anjali

0 Kudos