Hello,
I want to drive 2*16 LCD with MCUXpresso.How can I do it?
Hi Mutullah Eşer,
You can refer the 'Driving 16x2 LCD using KSDK drivers' first, although the version of SDK and IDE are different.
Then you can download the SDK_2.2_FRDM-KV10Z package refer Generating a downloadable MCUXpresso SDK v.2 package.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi Robin,
I had have already SDK and I'm using my frdm board.I want to learn
MCUXpresso have or not special library for 2*16 display.For example I want
to wirte on screen KSB what code can I write using.
Thank you..
Mutullah Eşer
KSB TURKEY
RD Engineer
2017-10-18 6:22 GMT+03:00 Robin_Shen <admin@community.nxp.com>:
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: Driving 2*16 LCD with FRDM KV10Z
reply from Robin_Shen
<https://community.nxp.com/people/Robin_Shen?et=watches.email.thread> in *MCUXpresso
IDE* - View the full discussion
<https://community.nxp.com/message/953050?commentID=953050&et=watches.email.thread#comment-953050>
The MCUXpresso SDK didn't have a special library for 2*16 display.
And I don't quite sure what does 'screen KSB' mean?
Maybe you can read 'HD44780 2x16 Character Display for Kinetis and Freedom Board' although it was not using MCUXpresso SDK.
Best Regards,
Robin
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------