Driving 2*16 LCD with FRDM KV10Z

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Driving 2*16 LCD with FRDM KV10Z

1,204 次查看
mutullaheser
Contributor I

Hello, 

 I want to drive 2*16 LCD with MCUXpresso.How can I do it?

0 项奖励
回复
3 回复数

720 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Mutullah Eşer,

You can refer the 'Driving 16x2 LCD using KSDK drivers' first, although the version of SDK and IDE are different.

Then you can download the SDK_2.2_FRDM-KV10Z package refer Generating a downloadable MCUXpresso SDK v.2 package.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复

720 次查看
mutullaheser
Contributor I

Hi Robin,

I had have already SDK and I'm using my frdm board.I want to learn

MCUXpresso have or not special library for 2*16 display.For example I want

to wirte on screen KSB what code can I write using.

Thank you..

Mutullah Eşer

KSB TURKEY

RD Engineer

2017-10-18 6:22 GMT+03:00 Robin_Shen <admin@community.nxp.com>:

NXP Community

<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>

Re: Driving 2*16 LCD with FRDM KV10Z

reply from Robin_Shen

<https://community.nxp.com/people/Robin_Shen?et=watches.email.thread> in *MCUXpresso

IDE* - View the full discussion

<https://community.nxp.com/message/953050?commentID=953050&et=watches.email.thread#comment-953050>

0 项奖励
回复

720 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

The MCUXpresso SDK didn't have a special library for 2*16 display.

And I don't quite sure what does 'screen KSB' mean?

Maybe you can read 'HD44780 2x16 Character Display for Kinetis and Freedom Board' although it was not using MCUXpresso SDK.

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复