Debian package of MCUXpresso IDE requires udev

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Debian package of MCUXpresso IDE requires udev

368 Views
stefanct
Contributor III

mcuxpressoide-11.9.0_2144.x86_64.deb executes `udevadm` as part of its `postinst` script. This command is installed with the `udev` pacakges, which might not be the case... such as with the default Docker image of Debian 12 because it simply does not make any sense there really.

I would prefer the compiler to be shipped individually without such shenanigans instead of together with Eclipse anyway. However, if the package actually requires it, it should depend on it, which it currently does not.

Tags (1)
0 Kudos
Reply
1 Reply

353 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @stefanct,

Thanks for reporting this. I will deliberate about this topic with internal to see what changes can be made or how to optimize the unnecessary packages.

BR,
Edwin.

0 Kudos
Reply