Hello, I use MCUXpresso IDE, and I try to compile a new created project or import SDK example project, it always fail. Please find below information:
It always shows: make: echo: Command not found
10:44:44 **** Build of configuration Debug for project MKE15Z256xxx7_Project ****
make -r -j4 all
0 [main] make 9328 proc_subproc: Couldn't duplicate child handle for pid 0, Win32 error 6
355 [main] make 9328 proc_subproc: Couldn't duplicate my handle<0x7C> for pid 0, Win32 error 87
7783 [proc] make 9328 wait_subproc: wait failed. nchildren 1, wait 1000, Win32 error 6
8351 [proc] make 9328 wait_subproc: nchildren 1, event[1] 0x0, pchildren[0] 0x2AA0000, events[0] 0x1A8, Win32 error 6
8726 [proc] make 9328 wait_subproc: pid 0, dwProcessId 0, hProcess 0x0, progname 'C:\NXP\MCUXpressoIDE_10.0.0_344\ide\msys\bin\sh.exe'
make: echo: Command not found
88342 [main] make 9328 proc_subproc: Couldn't duplicate child handle for pid 0, Win32 error 6
88352 [main] make 9328 proc_subproc: Couldn't duplicate my handle<0x7C> for pid 0, Win32 error 87
make: echo: Command not found
159667 [main] make 9328 proc_subproc: Couldn't duplicate child handle for pid 0, Win32 error 6
159680 [main] make 9328 proc_subproc: Couldn't duplicate my handle<0x7C> for pid 0, Win32 error 87
make: echo: Command not found
Building file: ../source/clock_config.c
Command canceled
10:45:25 Build Cancelled (took 41s.456ms)
Hi Alice,
Problem has been solved. After installing MCUXpresso, need to restart the computer, or it has this kind of error. thanks!
Best Regards,
Shaowei Su
There should be no need to restart a Windows PC after installing MCUXpresso IDE. And we have certainly not seen any similar errors reported in the past (with MCUXpresso IDE during development or with the previous LPCXpresso IDE). So I'm not sure what is going on here. But I am glad to hear that you are now up and running.
Regards,
MCUXpresso IDE Support
Hello Shaowei,
Please first install an SDK into MCUXpresso IDE.
The detail steps please refer to "MCUXpresso IDE User Guide"
4.4 Installing an SDK and 5. Creating New projects using SDKs .
If still have error , please show your steps .
Hope it helps
Have a great day,
Alice Yang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------