Can't install plugins on newest MCUXpresso IDE version 11.0.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can't install plugins on newest MCUXpresso IDE version 11.0.1

1,348 Views
miguel_perezand
Contributor II

I've recently asked this question. Digging a little bit, I discovered the problem is with MCUXpresso IDE 11.0.1. The plugins can be installed in the last version 11.0.0. This is the error I'm getting:

An error occurred while collecting items to be installed
session context was:(profile=DefaultProfile, phase=org.eclipse.equinox.internal.p2.engine.phases.Collect, operand=, action=).
No repository found containing: binary,MCUXpressoIDE.executable.gtk.linux.x86_64,11.0.0.201908271452

I don't know if this is a backward compatibilty error of the IDE or a bad configuration on the plugin providers' servers. Any help is appreciated, I want to use the newest version but this is stopping me.

Labels (1)
Tags (1)
0 Kudos
2 Replies

1,138 Views
lpcxpresso_supp
NXP Employee
NXP Employee

First point to note - we don't support MCUXpresso IDE on Fedora, we only develop and test on "recent" Ubuntu LTS releases. But that aside, one thing to try might be to start the IDE using sudo.

Regards,

MCUXpresso IDE Support

1,138 Views
miguel_perezand
Contributor II

It was solved by running as root. Thanks for your help.

0 Kudos