Can not launch the debugger on MCUXpresso 11.1.1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can not launch the debugger on MCUXpresso 11.1.1

3,910 Views
zhongshen
Contributor III

I just install the latest MCUXpresso IDE (MCUXpresso IDE v11.1.1 [Build 3241] [2020-03-02]) on my 64bits win10 surface pro 4. And importing a SDK sample for FRDM-KE06Z board, then make it is OK, but when I debug it I got the problem as picture show. And for check the hardware problem, I used KDS ( installed the same computer) to make a sample for same board, it is OK for the debug. Could you advise me how to fix this problem? Thanks.

pastedImage_2.png

pastedImage_3.png

pastedImage_4.png

0 Kudos
Reply
11 Replies

3,599 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hellozhongshen‌,

Just to confirm, 

If you update the FRDM-KE06Z debugger firmware from  OpenSDA Serial and Debug Adapter | NXP (download PE  or  CMSIS-DAP or segger) and then debug on a new project for the KE06 the same issue keeps appearing ?

Regards, Diego

0 Kudos
Reply

3,599 Views
zhongshen
Contributor III

Hi Diego,

Thanks for your help.

I try to use these three firmware, "P&E Micro v118", "CMSIS-Segger Jlink V1" and "DAP Debug Application for OpenSDAv1".

Here is the result. PE Micro V118 has the same problem as above;  OpenSDAv1 ( download from https://www.nxp.com/assets/downloads/data/en/reference-applications/CMSIS-DAP-OpenSDA.zip ) only has about 32KB size of CMSIS-DAP_OpenSDA.S19, I am not should that is the correct firmware which has the problem MCUXpresso IDE both of win10 and linux platform( see the following pics ). The Jlink V1 ( download from https://www.segger.com/downloads/jlink/OpenSDA_FRDM-KE06Z ) is worked OK on MCUXpresso IDE.

pastedImage_607.png

Console information:

MCUXpresso IDE RedlinkMulti Driver v11.1 (Feb 24 2020 13:54:38 - crt_emu_cm_redlink build 11)
Found part description in XML file MKE06Z4_internal.xml
Reconnected to existing LinkServer process.
============= SCRIPT: kinetisconnect.scp =============
Kinetis Connect Script
Connecting to Probe Index = 1
This probe = 1
This TAP = 0
This core = 0
DpID = 0BC11477
Assert NRESET
Reset pin state: 00
Power up Debug
MDM-AP APID: 0x001C0020
MDM-AP System Reset/Hold Reset/Debug Request
MDM-AP Control: 0x0000001C
Flash Not Ready
============= END SCRIPT =============================
Probe Firmware: OpenSDA CMSIS-DAP (Keil Software)
Serial Number: A000000001
VID:PID: C251:F002
USB Path: \\?\hid#vid_c251&pid_f002#6&12939929&0&0000#{4d1e55b2-f16f-11cf-88cb-001111000030}
Using memory from core 0 after searching for a good core
Cannot halt processor
Request debug reset of DAP
Cannot halt processor
Request debug reset of DAP
( 40) No Halt
debug interface type = Cortex-M0+ (DAP DP ID 0BC11477) over SWD TAP 0
processor type = Cortex-M0+ (CPU ID 00000C60) on DAP AP 0
number of h/w breakpoints = 2
number of flash patches = 0
number of h/w watchpoints = 2
Probe(0): Connected&Reset. DpID: 0BC11477. CpuID: 00000C60. Info: <None>
Debug protocol: SWD. RTCK: Disabled. Vector catch: Disabled.
Content of CoreSight Debug ROM(s):
RBASE F0002000: CID B105100D PID 000008E000 ROM (type 0x1)
ROM 1 E00FF000: CID B105100D PID 04000BB4C0 ROM (type 0x1)
ROM 2 E000E000: CID B105E00D PID 04000BB008 Gen SCS (type 0x0)
ROM 2 E0001000: CID B105E00D PID 04000BB00A Gen DWT (type 0x0)
ROM 2 E0002000: CID B105E00D PID 04000BB00B Gen FPB (type 0x0)
Cannot halt processor
Failed on chip setup: Ep(04). Cannot halt processor.

0 Kudos
Reply

3,599 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi @Zhong_Shen

 If I understand correctly, you were able to debug with J Link firmware. 

 

Regarding the error message,   is due to previously  active debug configurations.  You could follow the tips provided by our colleague Erich Styger on the following thread GDB Debugging with Kinetis Design Studio  under section  Troubleshooting

I hope this helps you. 

Best regards, Diego. 

0 Kudos
Reply

3,598 Views
renlei
Contributor I

Hi Diego

I have encountered some problems when using frdm-kw36, and I need your help.When I use LS or PE debug, the MCUXpresso IDE prompt is shown in the figure.The figure  shows debug using PE.But I was successful in erasing and programming frdm-kw36.Just debug doesn't work.pastedImage_5.pngPE.jpg

Best regards!

0 Kudos
Reply

3,599 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi Ren ,

Sorry for the delay.

It seems that the error  Target remote localhost:7224 appears if the GDB server cannot be found or if there is something wrong on the launch configuration.

You may already have found and test some of the following recommendations , but I will summarize them: 

For example with  PEmicro, check  to have proper target (in my case KL03Z),  and flash algoritm:

pastedImage_4.png

Coul you help me with the following inquiries:

  1. Were you able to debug previously, using the same MCUxpresso  and driver versions?
  2. Besides the other recommedations on thist  post,  there are other recovery paths you evaluated previously without sucess?

Best regards, Diego.

0 Kudos
Reply

3,599 Views
renlei
Contributor I

Hi Diego charles

Thank you for your reply. I haven't had this problem before, but it's true of every development board I've encountered recently.The same problem occurred on my computer and my colleagues' computers. I tried LS, PE and Jlink, but none of them worked.I don't know what to do anymore.The following is the error message for Jlink debugging.

SEGGER j-link GDB Server V6.44 I Command Line Version

Compiled May 17 2019 17:34:22 jlinkarm.dll V6.44 I (compiled May 17 2019 17:34:22)

The Command line:-nosilent -swoport 2332 -select USB=59611220 -telnetport 2333 - singlerun-endian little-noir-speed auto-rtos GDBServer/ rtosplugin_freeros-port 2331-powertarget 50-vd-device mkw36z512xxx4-ifSWD - the halt - reportuseraction

-- -- -- -- -- the GDB Server start Settings -- -- -- -- --

GDBInit file: none

GDB Server Listening port: 2331

SWO raw output listening port: 2332

Terminal I/O port: 2333

Accept remote connection: localhost only

The Generate logfile: off

Verify the download: on

Init regs on start: off

Silent mode: off

Use the run mode: on

Target connection timeout: 0 ms

-- -- -- -- -- - J - Link related Settings -- -- -- -- -- -

J - Link Host interface: USB

J - Link script: none

J - Link Settings file: none

-- -- -- -- -- - the Target related Settings -- -- -- -- -- -

The Target device: MKW36Z512xxx4

Target interface: SWD

Target interface speed: auto

Target endian: a little

Connecting to J - Link...

J - the Link is connected.

Device "MKW36Z512XXX4" selected.

Firmware: j-link V9 compiled May 17 2019 09:50:41

The Hardware: V9.60

S/N: 59611220

Feature(s): RDI, GDB, FlashDL, FlashBP, JFlash

Checking target voltage...

Target voltage: 3.35 V

Listening on TCP/IP port 2331

Connecting to the target...InitTarget ()

The Connect Under the Reset

Communication error while ss -AP.

The Connect Under the Reset

InitTarget ()

The Connect Under the Reset

Communication error while ss -AP.

The Connect Under the Reset

ERROR: InitTarget(): PCode returned with ERROR code-1

InitTarget ()

The Connect Under the Reset

Communication error while ss -AP.

The Connect Under the Reset

InitTarget ()

The Connect Under the Reset

Communication error while ss -AP.

The Connect Under the Reset

ERROR: InitTarget(): PCode returned with ERROR code-1

ERROR: Could not connect to target.

Target connection failed. GDBServer will be closed...Restoring the target state and closing J - Link connection...

Shutting down...

Could not connect to target.

Please check power, connection and Settings.

The Server has been shut down.MCUXpresso IDEWireless Connectivity

0 Kudos
Reply

3,599 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi ren,

Sorry for the delay,

 

First , make sure that the board is not bricked  by  erasing  the board  K20 debug probe and then loading the binary file. For this an external debug probe is required. For details on this go to   Freedom OpenSDA Firmware Issues Reported on Windows 10.

Then ,  try to  check if you are able to perform and erase on the target MCU (KW36) . Here are two ways for doing this:

  •  A) In MCUxpresso, go to GUI flash tool and go to Resurect locked device, then  erase the flash memory.

pastedImage_4.png

  • B)  Use J-link commander and connect to the target (KW36), then use commands unlock kinetis and erase

unlock_commad_example.PNG

If you are not able to perform this, please let me know.

Regards,

Diego

0 Kudos
Reply

3,599 Views
renlei
Contributor I

Hi Diego Charles

Thanks for your reply!

When I use LS, I can Resurect locked device& erase, but when I use Jlink, I cannot Resurect locked device.I also tried Jlink commander, but I still couldn't connect to core.And no matter what method I use, I can't debug.

pastedImage_4.png

0 Kudos
Reply

3,599 Views
diego_charles
NXP TechSupport
NXP TechSupport

Hi Ren,

I apologize for my abscence!

Thank you for providing your output, However I will have to check with my colleagues. 

In the meantime, could you help me with the following?

  • Create a new path close to the C disk and debug on a blinky project, for exaple:   C:/MCUs/blinky .
  • Check with an external debugger  if you are able to debug by SWD or JTAG
  • Provide the error log obtained when you are not able to perform  mass erase with J-link.

Regards, Diego

0 Kudos
Reply

3,598 Views
zhongshen
Contributor III

Thanks for you comments.

Delete all launch configurations, and using blue Debug button to start debug. The problem is still existed even reinstall IDE again!

And I try to use a example in SDK for FRDM-KL25Z board, it is OK to launch debug. The OpenSDA version is different: Application Version is: 1.18 on FRDM-KE06Z board and Application Version is: 1.14 on FRDM-KL25Z board.

On linux desktop, MCUXpresso 11.1.0 is OK to launch debug for FRDM-KE06Z board. It is only in windows MCUXpresso 11.1.1 could not launch debug for FRDM-KE06Z board.

pastedImage_2.png

pastedImage_3.png

0 Kudos
Reply

3,598 Views
converse
Senior Contributor V

Starting debug in MCUXpresso is different to the way you do it in KDS. So delete any launch configuration that you may have created, and start debug using the blue Debug button that is in the QuickStart panel. This is described in the User Guide.

0 Kudos
Reply