Board SDK configuring board flash driver

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Board SDK configuring board flash driver

ソリューションへジャンプ
2,543件の閲覧回数
mperez1
Contributor II

Hello there,

We are trying to develop a custom board with the IMXRT1050 mcu, for that we followed the webinar training Creating a Custom Board SDK and Migrating Code Between Boards | NXP. Everything worked perfectly and now we are trying to add new examples to the Board SDK. In order to achieve that, we have to configure the Flash and RAM configuration of the board and then the problems started. 

We have a similar flash configuration with the Evaluation Board, so when we added the HyperFlash driver and try to add a new example we receive a JavaNullPointer exception. 

If we remove the BOARD_FLASH line the NullPointer exception disappered when we include a new example. When we added the BOARD_FLASH line the Board SDK added a linked file to this driver, we removed this linked file and added the original file without any success. 

Anyone faced the same problem and could solved it? There is really few documentation of this topics and we don´t know how to continue.

Thank you everyone for the help.

pastedImage_2.png

pastedImage_4.png

タグ(1)
0 件の賞賛
返信
1 解決策
2,335件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Hi Miguel,

Thanks for reporting the problem.

The fix for this topic will be available in the next build - MCUXpresso IDE 11.2.1.

Greetings,
MCUXpresso IDE Support

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
2,391件の閲覧回数
mperez1
Contributor II

Hello,

There is any news on this topic?

Regards,

Miguel

0 件の賞賛
返信
2,336件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Hi Miguel,

Thanks for reporting the problem.

The fix for this topic will be available in the next build - MCUXpresso IDE 11.2.1.

Greetings,
MCUXpresso IDE Support

0 件の賞賛
返信
2,395件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi Miguel,

the most update IDE version is 11.2. Can you please try it?

Regards,

Jing

0 件の賞賛
返信
2,395件の閲覧回数
mperez1
Contributor II

Hello Jing,

Thank you for answering I forgot to tell it, but I´m already using the 11.2 IDE version.

Regards,

Miguel

0 件の賞賛
返信
2,395件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Would you please send us .log file from your workspace? That should give us some indications about the NPE. Alternatively, we now have an easier way to export data for diagnostics and send it to us - see screenshot.

pastedImage_1.png

Meanwhile, we'll see if we can reproduce the described behavior.

Greetings,
MCUXpresso IDE Support

0 件の賞賛
返信
2,395件の閲覧回数
mperez1
Contributor II

Hi,

Thank you for the support.

I attach the project that I'm trying to add as example and the custom board SDK as "Support_Project_and_custom_SDK.zip". Also, in another zip, there is the log support generated by MCUXpresso as "2020070301231_SupportInfo.zip".

Regards,

Miguel

0 件の賞賛
返信
2,395件の閲覧回数
lpcxpresso_supp
NXP Employee
NXP Employee

Thank you. We'll look into this.

Greetings,
MCUXpresso IDE Support

0 件の賞賛
返信
2,395件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi,

Can you share your project and custom board sdk?

Regards,

Jing

0 件の賞賛
返信