mcuxpresso ide问题

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

mcuxpresso ide问题

1,418件の閲覧回数
zhuijun
Contributor I
  1. 最近在学习mcuxpresso ide和cortex-m微处理器的开发,有些问题希望得到帮助,我使用ide是v11.1.0,使用的sdk是lpc54114j256的v2.7, 使用的config tools 是v7.0(Peripherals v7.0)我发现我在sdk中导入的例子,如The uart_functioncal_interrupt example,我发现我在peripherals中设置的内容和例子中的不匹配。
  2. 我找不到sdk中提供的api和config tools中自动产生的代码的关系,特别是串口中断和回调函数之间的关系
  3. 我也找不到相关的文档来说明这些问题,我看了一些sdk api reference和config tool的帮助文档,没有发现相关内容
ラベル(1)
タグ(1)
0 件の賞賛
3 返答(返信)

1,216件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi

If you use MCUXpresso IDE v11.1.0, please use the config tools inside the IDE rather than the standalone Config tool.

We can enable config tool from IDE this way:

pastedImage_1.png

then enter the config tool. After finishing the config, click on update code.

pastedImage_2.png

if you want to where is changed, click on "click"

pastedImage_3.png

Have a great day,
Jun Zhang

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

1,216件の閲覧回数
zhuijun
Contributor I

谢谢,我刚刚开始使用mcuXpresso ide,很多操作还不熟悉,谢谢您的帮助,此外,mcuxpresso ide可以支持rt-thread的工程吗?

我在网上搜索了一下,还真找不到相关资料。

0 件の賞賛

1,216件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

Our engineer will answer your additional question in 

https://community.nxp.com/thread/524175 

Thanks,

Jun Zhang

0 件の賞賛