Hi,
I'm not able to view the MCUXpresso training videos from the 'debugging series' like:
(and the other: part 2,3,4 etc.)
The video doesn't show even the 'play' icon. While right clicking I can see that it uses Brightcove Player Version 6.45.4 and Video.js Version 7.9.3.
On the other hand I have no problems with playing the content with other training videos whenever the Brightcove Player Version is 6.46.4 and Video.js Version 7.9.7.
It's the same with latest Chrome and Firefox browsers.
How can I view these training videos ?
Regards
Maciek
已解决! 转到解答。
Hi @Maciek :
I f tried this link on my side , found this link is working with Google Chrome now.
Regards
Daniel
Hi @danielchen ,
In the meantime I've found another problem with training videos - some of them are playable but the video itself is not resizable (I'm not able to enter full-screen mode) and there are no usual controls like 'forward/backward', 'full-screen', 'stop/play' etc. You can only pause/resume the video using 'space' key.
Look for example here (I've found many other videos with the same bahavior):
In many cases the small vewing area is not readable enough to be useful. Is this a problem at NXP site or I'm not able to use the embedded player correctly ?
Thanks for help
Maciek
It is a bit odd, but this is what I found works:
play the video - there now appears a pause control on the right of the video (along with options to play 2 other videos). press it
now press play again, and the video now goes full screen, together with all of the standard pause/forward/reverse/etc controls
Thanks for your suggestion but it doesn't work in my case. In latest Chrome and Edge I have the same behavior: when clicked once - the play icon (on the right of the video window) changes to 'pause' and any subsequent clicking doesn't change it any more - it simply restarts the whole video from the beggining.
As I said - it's not usable at all. Does anyone know what versions of OS/browser/etc. (or some other dependencies) are required to view these videos ?
Maciek
Thanks @danielchen,
I was constantly checking NXP training site and have found a week (or so) ago that the links are finally fixed. Now all the videos seem to work fine and I use them frequently.
Regards
Maciek